AXIS#.MOTOR​.BRAKEPOWERDELAY

Description

Time to wait after applying full voltage before dropping to low voltage when AXIS#.MOTOR​.BRAKEPOWERSAVING = 1.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

0 to 2000

Default Value

150

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.